5/23/2014 4:23 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
Hello, following an example how to configure Bit15 in PZD 12 as triggerbit. AttachmentD:\temp\Bitpattern.pdf (143 Downloads) |
Last edited by: TechTeam at: 5/23/2014 4:24 PMWith best regards, |
|
5/23/2014 6:07 PM | |
Joined: 3/15/2011 Last visit: 9/18/2024 Posts: 134 Rating: (9) |
Hello everyone. I would like to implement recording of position/speed of my motor in Starter. However, the recording should start on signal from PLC. How can I implement this? I have Sinamics S120 (it has TM31) and S7-1500. Couldn't find anything on internet. Thanks. Hi, In addition to what Tech Team said, don't forget to enable the trace function,as attached below regards Ashutosh
Attachmentdrive_trace_1.pdf (103 Downloads) |
5/24/2014 12:34 PM | |
Posts: 87 Rating: (1) |
Can I use PZD 12 of Siemens telegram 111 to turn on tracing? In manual it says it is reserved, but I am not sure what that means. |
5/26/2014 3:33 PM | |
Posts: 87 Rating: (1) |
Can anyone explain how can I modify Bit pattern and Bit mask so if I change 47e to 47f in PZD 1 that my recording turns on? |
5/26/2014 4:16 PM | |
Joined: 10/10/2010 Last visit: 9/14/2024 Posts: 307 Rating: (15) |
try to read the advanced manual of how to set the comunication control word and status word telegram |
Follow us on