9/15/2014 12:17 AM | |
Posts: 13 Rating: (0) |
Hi, I have this project going on: http://youtu.be/1Wqk2uQuAqw Now there are 2 files in attachment: An .xls and a .lsc file. The .lsc file is doing well in the youtube movie. But now i need to convert the .lsc file according to the detail in the .xls file,-I made to clarify. ( 2 tabs). Can someone help me on the way, cause its a lot more difficult, beyond i learned so far. A second problem is, that when i push the STOP button at sequence for example "23", then after pushing the start button, the cycle needs to restart at "24". Now each time i push the STOP- button, afterwards the cycle restarts at "1". I hope someone has the insite to understand the sequences with the files attached, because its to much to explain in words here on this forum...i made them especially for this question. Thx very much in advance for a specialist to look in to my LOGO! problem. ps: nice machine isn't it? Kind Regards Filip Elgers AttachmentForum Siemens.zip (202 Downloads) |
Last edited by: Dragonaut at: 9/15/2014 12:17 AM |
|
9/15/2014 12:30 AM | |
Posts: 13 Rating: (0) |
A little adjustment to the colours of the sequences in the .xlsx file. sorry. AttachmentForum Siemens.zip (205 Downloads) |
9/15/2014 10:32 AM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (715)
|
Hello, The 2nd question: Pushing the stop button resets your counters, so it will start from 0 again. Remove the connection Stop button ----->B18 (OR) But now your outputs stay on, if that's not wanted, add a AND block to every output wire to B17(RS) and whatever sets the output. I have attached the modyfied program. Regards, Marcjan AttachmentK2-2- testfase 14092014 met knop schacht - 64_2_1.zip (222 Downloads) |
Last edited by: Marcjan at: 9/15/2014 11:20 AMForgot the manual controls, corrected. Problem solved? |
|
Follow us on