6/19/2017 10:56 AM | |
Posts: 5 Rating: (0) |
Hello! There is a program Starter 4.3.3 with SSP v1.4 and converter 6RA8025-6D22-0AA0 with version 1.4.1. The program for this drive requests another SSP. Where can I get it? Or should I install Starter of a higher version? ------------------------------------------------------------------------------------------ |
Last edited by: ingenersbp at: 6/19/2017 11:00:30 AMLast edited by: Min_Moderator at: 6/21/2017 10:45:18 AMNew subject after splitting |
|
6/19/2017 11:37 AM | |
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983) |
Hello, you must update you STARTER. If you update to Starter V4.5 then the SSP is included in the Starter Setup https://support.industry.siemens.com/cs/ww/en/view/26233208 For Starter V4.3 is no SSP for DCM V1.4 SP1 available. Regards Christoph |
6/19/2017 11:59 AM | |
Posts: 5 Rating: (0) |
|
Last edited by: ingenersbp at: 6/19/2017 12:02:19 PMLast edited by: ingenersbp at: 6/19/2017 12:02:39 PMLast edited by: ingenersbp at: 6/19/2017 12:04:46 PM |
|
6/19/2017 12:08 PM | |
Posts: 5 Rating: (0) |
Can I put Starter 4.4 on Windows XP SP 3? There is DCM V1.4 SP1 |
6/19/2017 12:14 PM | |
Posts: 5 Rating: (0) |
To install Starter 4.4, do you need to uninstall Starter 4.3? |
6/19/2017 12:21 PM | |
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983) |
Hello, yes V4.4 SP1 is the last version with Windows XP Support The DCM V1.4 SP1 SSP is included in STARTER V4.4 SP1 and yes you should uninstall STARTER V4.3 before you install STARTER V4.4 SP1.
|
6/19/2017 12:24 PM | |
Posts: 5 Rating: (0) |
The project created in Starter 4.3 will open in Starter 4.4? |
6/19/2017 12:45 PM | |
Joined: 5/12/2006 Last visit: 5/13/2024 Posts: 22244 Rating: (2983) |
yes |
Follow us on