Industry Online Support
Technical Forum
6/20/2016 12:16 PM | |
Posts: 2 Rating: (0) |
I have a challnge with a CPU from one field instrument which is connected to the PLC.When i open the CPU it is in run mode but status has a red slash and a message saying module configured but not available.The instruments is there in the field and profibus is connected.Please help. ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 6/20/2016 5:05:14 PMNew subject after splitting |
|
6/21/2016 10:35 AM | |
Joined: 4/28/2015 Last visit: 2/7/2024 Posts: 10533 Rating: (818) |
Hello, can you post pls Picture, we can better look to problem. |
With best regards... |
|
Follow us on