6/20/2017 9:28 PM | |
Posts: 2 Rating: (0) |
Hello all, After a change on the code, when the program was downloaded the "blocks" called by the program stopped to work properly. We try to donwload again the FB and still with error. This PC that we were using, when we open the FB generate the error 257:8 ( see picture Step 7 Error 257_8.jpg) To correc the issue we opened the same previous backup but on another machine ( that have all the packages ), downloaded just the FC1230 and it started to work again. See the pictures where we compare both programs, one from the PC that was generating the issue and the other from another PC with all the packages. ( " PLC compare FC1230 Nw 8_Commented.jpg " and " compare FC1230 Nw 8_Comented.jpg") As you can see on the prints, on the software that had the issue, looks like that the TAGS from temporary memories ( L27.X) were "Shifted" to another memory position (L28.X) and all the following memories follow this "shift". We want to know if this error ( 257:8 ) cound generate the "shifting" from the memories. Or wat could cause it.. Regards and thanks for the help AttachmentSTL Error.pdf (89 Downloads) |
6/21/2017 5:59 AM | |
Joined: 12/9/2010 Last visit: 10/8/2022 Posts: 623 Rating: (76) |
Hi Tiagoebeh, Do 'compile all' function for entitre program. Also Reorganize -slow for automatically updating time stamps. |
If you like the comment, rate it (right top) or thank it (left bottom). |
|
Follow us on