8/3/2012 9:24 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hallo, it is not a problem to use WinCC V11 SP2 together with STEP 7 V11 SP1. The linceses refers only the the kind of versions. Not to service pack. For each STEP 7 version you need the apply linceses. See in this case the FAQ: http://support.automation.siemens.com/WW/view/de/57775228 Regarding the SP2 for STEP 7 V11 you can this download from the internet. See the following link: http://support.automation.siemens.com/WW/view/de/56771572?Datakey=56771572 Mit freundlichem Gruß |