Industry Online Support
Technical Forum
2/17/2006 12:36 PM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, regarding to your inquiry we would like to inform you. Please consider, if you have installed STEP 7 Basic V5.1, you can not install STEP 7 V5.2 or V5.3 Professional. You have to deinstall STEP 7 V5.1 complete and delete in this case the registry files. In refer to the deinstallation of STEP 7 pleasemake all the steps which are described in the FAQ "Complete Deinstallation of STEP 7", which do you will find by Beitrags-ID: 189025. The FAQ you will find by the customer support of Siemens: http://www.siemens.com/automation/csi_en/product After the complete deinstallation you can install the STEP 7 Professional V5.2 or V5.3. With best regards Cicero |
Follow us on