2/15/2012 4:48 PM | |
Joined: 2/15/2012 Last visit: 8/23/2024 Posts: 56 Rating: (12) |
Hi Everyone, When installing STEP7 on a vmware workstation 8 running XP SP3, the installation procedure hangs. The service s7oiehsx blocks and uses 25% of my CPU. When i ignore the errors, all works fine until i whant to go online via ehternet, sometimes the communication server fails and ik have to restart the virtual machine. I asked also the question at http://communities.vmware.com/message/1989279 for all details Yes i know that siemens doens't support the vmware, and i know there are people who are using this successfully with STEP7. (I am using STEP7 SP5 and WinCC flexible) My question: What does the S7oiehsx service exacly? I know it is opening the iso-tsap port on my pc and it is the process "s7oiehsx.exe+0xc66cc" that is causing the delay. Thanks in advance, Coldrestart. |
2/16/2012 8:43 AM | |
Joined: 2/15/2012 Last visit: 8/23/2024 Posts: 56 Rating: (12) |
Hi, The setup just "hangs" so i don't have any error's.Once i killed the process, the setup continous. I also tested it with windows XP SP2 Here some screenshots of proces explorer, as you can see it opens port 102, so i don't think it is just the "help" function, it is IEPG helper -> PG -> communications? I had crashing communication when i go online via ehternet. When i have that error, i will post the error message. Can you give your exact configuration -> windows + installed S7 software with versions? Kind regards Attachmentscreenshots.zip (339 Downloads) |
2/22/2012 9:14 AM | |
Joined: 10/10/2005 Last visit: 8/29/2024 Posts: 1917 Rating: (136) |
Hello, please find the FAQ (link) with the informations and hints. This could be meanful for the future if you want to install the STEP 7 software again. http://support.automation.siemens.com/WW/view/de/23568401 With best regards |
Follow us on