2/29/2012 4:02 PM | |
Joined: 2/15/2012 Last visit: 4/11/2024 Posts: 56 Rating: (12) |
Hi, First of all, windows HOME edition is always tricky -> siemens doesn't support it. But no worry, you are running a virtual machine, as long as that system is a professional XPedition. I use windows XP mode, it's free from microsoft: http://www.microsoft.com/windows/virtual-pc/download.aspx For your USB adapter use the NEW drivers 2.0! Not the 1.2 version. Kind regards. |
6/28/2012 5:07 PM | |
Joined: 6/28/2012 Last visit: 4/22/2024 Posts: 1 Rating: (1) |
VMware Solution: Max CPU usage by S7oiehsx.exe and S7epatsx.exe appears to be related to a change in the VM BIOS (this was not an issue with Workstation 7). Workstation 8's version of the BIOS allows for more CPUs and RAM. Extract the VM BIOS from Workstation 7, then change your VM's settings to use the version 7 BIOS. Running in 8 with a 7 BIOS eliminates the problem. See: http://pete.akeo.ie/2011/06/extracting-and-using-modified-vmware.html Fix/Workaround confirmed with: STEP 7 V5.3 SP2 HF15 STEP 7 V5.4 SP4 HF6 |
This contribution was helpful to3 thankful Users |
Follow us on