4/7/2009 4:22 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Serk, Look at What are the requirements for installing STEP 7 version 5.4? . Your hardware and software is enough. I suggest you only to upgrade to v.5.4 plus upgrade license. About corrupted licenses, don't wory, it's only necessary to contact with Siemens Hotline and they will prepare knew one. Hope this will helps. Best regards |
This contribution was helpful to1 thankful Users |
4/8/2009 9:54 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Dear Serk, When you want to upgrade to Step 7 v5.4 + sp4. You need first to upgrade Windows to Windows XP prof. , then you can install Step 7 v5.4 + sp4. See following link: http://support.automation.siemens.com/WW/view/en/29753194 Windows 2000 is not supported any more. Best regards, Wizard |
This contribution was helpful to1 thankful Users |
4/8/2009 1:14 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181) |
Hello Wizard, You are right. . But I think for Serk, v5.4 SP3.1 is the last and cheapest possibility to do upgrade of his PG. Even, I don't know if it would be possible to do other. Soon, maybe after Hannover, I expect to be released SP5, then maybe Serk is better to buy this new installation, of cource with change of OS. Best regards |
Last edited by: UMENCHO at: 4/8/2009 1:15 PMLast edited by: UMENCHO at: 4/8/2009 1:15 PM |
|
This contribution was helpful to1 thankful Users |
Follow us on