5/4/2016 10:46 AM | |
Joined: 2/11/2016 Last visit: 4/19/2024 Posts: 1 Rating: (0) |
Hello Pittiplatsch, I am working in Step7 V5.5 with a multiproject where I want to connect all plc's in 1 mrp-domain. But the "manager" is in the first project in PLC1 and all the other plc's are in other projects of this multiproject. Can you tell me how I can connect all these plc's in one ring-network? I Always get in Netpro the message: "Error: A manager must be configured in an MRP domain" I know this is correct because because the manager is in another plc, but it is not possible to connect all MRP-domains to 1 like you can do with the ethernet in a multiproject. And also: "Warning: Since the topology of the MRP-domain "mrp-domain-1" is not correctly configured, the consistency of the MRP domain cannot be checked" Can anybody help me with this problem? thanks ------------------------------------------------------------------------------------------ AttachmentNetworkOverview2.pdf (324 Downloads) |
Last edited by: Min_Moderator at: 5/4/2016 12:57:08 PMNew subject after splitting |
|
Follow us on