1/3/2013 8:29 AM | |
Posts: 21 Rating: (0) |
Hi again, Isn't there anybody to help me? I am struck here..Please Help. |
1/3/2013 1:42 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello arihant; I do not consider myself as an expert on S7-200 position control, but there is some information available on the subject. You will find the S7-200 System manual in the following link: http://support.automation.siemens.com/WW/view/en/1109582 Chapter 9 discusses open-loop position control, including the Postion wizard and the PTO control blocks. Examination of the different blocks will give you this type of detail: PTOx_MAN Subroutine The PTOx_MAN subroutine (Manual Mode) puts the PTO output in manual mode. This allows the motor to be started, stopped and run at different speeds within the range from Start/Stop speed through Maximum speed as specified in the wizard. Hope this helps, Daniel Chartier |
1/4/2013 12:06 PM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
closed cause question allready discussed within the thread Microstepping using S7 200within the same conference. Best regards CS Moderator |
My Forum is the place to personalize your profile, |
|
Follow us on