5/2/2010 2:43 PM | |
Posts: 11 Rating: (0) |
hj all, i want to know the meaning of following insts.(probably german ops) ep m 200.1 m fd m fw thnx for any advice |
5/2/2010 5:06 PM | |
Joined: 3/24/2009 Last visit: 7/9/2024 Posts: 535 Rating: (112) |
Dear ashwani, these instructions are not included in the international or german instruction-set. In the german instructionset EP is mentioned in an example on page 270, but I think, that this is a type-error and should be FP (positive edge). I can't say anything about M FD and M FW. Best regards yy1 |
5/2/2010 11:25 PM | |
Joined: 10/7/2005 Last visit: 9/24/2024 Posts: 3022 Rating: (1054)
|
Hello ashwani I agree with what yy1 said and as for the rest, let's just say it seems that a cat ran across the keyboard of the person who wrote the English manual and that the QA must have been on annual leave. Here's what it should be in English mnemonics: A M 200.0; FP M 200.1; JCN m001; L 0; TMD 100; TMW 104; TMW 106; R M 200.0; m001: NOP 0; Note that the logic could be optimised too if "T MD 104" instead of "TMW 104 &TMW 106"isused. I hope this helps |
Last edited by: fritz at: 5/3/2010 8:13 AMFixed up FW and FD to MW and MD Cheers |
|
5/3/2010 8:18 AM | |
Joined: 10/7/2005 Last visit: 9/24/2024 Posts: 3022 Rating: (1054)
|
That should of course have been MD and MW and I fixed up my previous post (I'm sometimes still too used to (english)S5 mnemonics whereMemory "bits" were called Flag"bits"). |
Cheers |
|
5/3/2010 9:31 AM | |
Posts: 11 Rating: (0) |
thnx fritz |
Follow us on