3/30/2016 11:32 AM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating: (193) |
Hello vadvikb, if you reference a documentation it would be helpful to write which one and to add a link and the page/ a screenshot. Maybe one of these FAQs helps?
|
~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
3/31/2016 9:53 AM | |
Joined: 1/23/2013 Last visit: 8/30/2023 Posts: 4 Rating: (0) |
Hello H.J. I set up the database according to the documentation But archiving stops going after 1-2 minutes after start runtime. After the restart runtime I can see previous archives for 1-2 minutes, but after 1-2 minutes stops archive again. No reports on this issue no. In the Windows event too. Resetting the system with zero result has not brought. I do not understand what's the matter???? Regards!! |
Last edited by: vadvikb at: 3/31/2016 9:57:49 AM |
|
6/10/2016 1:56 PM | |
Joined: 1/23/2013 Last visit: 8/30/2023 Posts: 4 Rating: (0) |
Problem is solved! Regards!!! |
Follow us on