9/5/2014 9:55 AM | |
Joined: 10/10/2005 Last visit: 4/18/2024 Posts: 1917 Rating: (132) |
Hello, it is possible, that the driver in refer to the online connection are not up to date. This is a basicly reason after an image installation. See in this case the FAQ: http://support.automation.siemens.com/WW/view/en/99005532 With best regards |
This contribution was helpful to2 thankful Users |
9/30/2014 5:21 PM | |
Joined: 9/3/2008 Last visit: 5/6/2024 Posts: 921 Rating: (158) |
Do you have VPN adapters installed on your computer? If so, can you deactivate them and try to see if it helps? |
Michael |
|
2/18/2015 5:23 PM | |
Posts: 91 Rating: (4) |
Thanks to Cicero for this one -- this was a weird one that was very hard to figure out what was wrong until I finally stumbled upon this thread. If you are having accessible device problems in TIA Portal - start here first. Or upgrade to TIA v13 SP1. |
Follow us on