6/20/2013 9:41 PM | |
Joined: 9/27/2006 Last visit: 4/23/2024 Posts: 12257 Rating: (2665)
|
Hello Peter; How are the sensors wired? Does your wiring match the following schematic (taken from the manual SIMATIC S7-300 S7-300 Module data)? That means 24 VDC power to pins 1 and 20 of the analog module, 24 VDCpower to each sensor, + and - signal inputs to unsused channels wired in series with the used ones... This lastinformation comes from the same chapter: 6.7.3 Additional information on SM 331; AI 8 x 12 Bit Unused channels … · Current measurement 4 mA to 20 mA, 4-wire transducer: wire the unused inputs of the same channel group in series. Hope this helps, Daniel chartier |
Last edited by: O_Moderator at: 6/21/2013 10:46 AMLast edited by: dchartier at: 6/20/2013 9:45 PM |
|
6/21/2013 10:44 AM | |
Posts: 11 Rating: (0) |
Hello, here are the wiring of the abb drive and the analog input. I don't think there is anything wrong with it. Greetings, Peter Attachmentwiring.zip (214 Downloads) |
Follow us on