6/6/2019 3:22 PM | |
Joined: 9/9/2015 Last visit: 9/15/2024 Posts: 727 Rating: (278) |
The strikethrough message should be gone when you retrigger the same message again. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
6/6/2019 5:10 PM | |
Joined: 8/1/2012 Last visit: 7/16/2024 Posts: 76 Rating: (3) |
Hi Hamid.Servat, Please see below post from Heisenberg, might help you https://support.industry.siemens.com/tf/WW/en/posts/alarms-strikethrough/10274?page=0
Regards, wantutri |
This contribution was helpful to1 thankful Users |
6/7/2019 1:25 PM | |
Joined: 8/14/2012 Last visit: 9/12/2024 Posts: 38 Rating: (4) |
thank you I read this post befor i creat this topic but it doesnt useful for my problem |
6/24/2019 1:38 PM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello Hamid.Servat, as wantrutri already wrote, the crossed-out date and time of a message are shown if the message in the automation system is already due while starting the process execution of the operator station. Date and time do not correspond with the date and time at which the message in the automation system resulted, that's not an issue. Something else is, when there are messages that can not be acknowledged. These message can appear when there is an active message in the runtime and the CPU loses the power. In this case it usually helps to restart the OS Runtime. However, you cannot always restart this, for example, when implementing a redundant server pair, when only one server can be shut down at a time. Then you can use the FAQ to delete the message. With an redundant OS server pair you can compile and load the OS server without to Stop. And why you can't compile the ES or OS?
If you compile Changes or Entire OS without the Option "With memory reset" the Alarm and Tag logging will not deleted. The Alarm and Tag logging will only delete if you selected the option "With memory reset". With regards |
This contribution was helpful to1 thankful Users |
7/31/2019 6:27 AM | |
Joined: 8/14/2012 Last visit: 9/12/2024 Posts: 38 Rating: (4) |
thank you for reply dear friend So i will try to delet old steriketrough message from my archive with own solution siemens Tnx a lot |
Follow us on