5/21/2016 12:06 PM | |
Joined: 2/15/2010 Last visit: 1/20/2024 Posts: 329 Rating: (6) |
Dear, CPU IS 316-2DP |
Hazem |
|
5/21/2016 12:28 PM | |
Joined: 3/30/2011 Last visit: 9/22/2024 Posts: 736 Rating: (256) |
Hello, if your cpu is 6ES7316-2AG00-0AB0 as you can see in technical data first interface is only mpi, second interface only profibus. Regards |
★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★★ |
|
5/22/2016 4:15 PM | |
Joined: 10/7/2005 Last visit: 9/25/2024 Posts: 3022 Rating: (1054)
|
A PG can also communicate with an S7 via Ethernet, but you won't be able to connect your DP Slaves to the PN port, would you? (well, you could via an additional PN/DP gateway but that is a different story). Anyhow, you can not connect DP Slaves to a pure MPI port of your CPU, end of the story (sorry, but it is what it is). |
Cheers |
|
This contribution was helpful to2 thankful Users |
Follow us on