6/9/2017 11:05 AM | |
Posts: 69 Rating: (0) |
Hi JDarius, I'm using the example image but tbh I can't tell you which version it is...:o BR |
6/9/2017 11:08 AM | |
Posts: 215 Rating: (6) |
See here. |
6/9/2017 11:22 AM | |
Posts: 69 Rating: (0) |
V2.1.2 |
6/9/2017 11:29 AM | |
Posts: 215 Rating: (6) |
Then the solution is easy. Get the latest image here and the problem should be solved. with the latest image, node-red will store the data in the same directory, independent from the start-up. So you will see the same flows, no matter whether it started automatically or manually. You should however save the flows and anything else you don't want to lose, since a new image version requires overwriting the old image. |
This contribution was helpful to2 thankful Users |
Follow us on