Industry Online Support
Technical Forum
6/23/2009 9:15 PM | |
Joined: 12/20/2008 Last visit: 8/12/2024 Posts: 556 Rating: (236) |
Where can I put the description to All my I/O, Is it Symbol Table, where do I need to put the I/O Description, Moreover weather or not the I/O description will be saved in PLC? Weather or not Symbol Itself will store in the memory of PLC, this is considering the fact I am using CPU315-2PN/DP with 128 K Ext mem card. I am attaching the program for refernce. AttachmentCT40629.zip (152 Downloads) |
6/23/2009 9:49 PM | |
Posts: 39 Rating: (3) |
Symbol table is stored only in off-line project. |
6/24/2009 2:12 AM | |
Posts: 1064 Rating: (72) |
You can store the files on the mcc as RIT03 said but remember to re-archive the project after changes as this is not automatic |
Follow us on