8/15/2014 7:04 PM | |
Posts: 767 Rating: (69) |
Hello C4ssius, From initial description of application needs, this type of angular synchronising between two different motors could be achieved with SINAMICS S120 drives and SIMOTICS Servo Motors in a few different ways. Following is a link which introduces SINAMICS Drive Control Block(DCB) Extension. SINAMICS DCB Extension is an extension option for SINAMICS Drive Control Chart(DCC) and included in the Advanced Technology Function of SINAMICS S120. This includes DCB blocks which have been created with the development environment SINAMICS DCB Studio. These blocks can be used in the SINAMICS DCC environment, analogously to standard blocks. SINAMICS DCB Extension would be an implementation where the synchronizing would be performed within the drive system. |
This contribution was helpful to1 thankful Users |