10/27/2015 3:04 PM | |
Joined: 4/14/2010 Last visit: 4/3/2024 Posts: 525 Rating: (11) |
Greeting, We want to synch the speed of two geared motors of conveyors without slippage because precision require in a millimeter, there is automatic engine supply conveyor between one engine assembly and one frame assembly as attached layout. Please suggest which type of motors and drives can done this Job..?? Geared Motor Specification: 0.37KW, Torque 1320Nm Output RPM 1.5 Regard's AttachmentAes conveyor.pdf (292 Downloads) |
MS |
|
1/22/2016 5:40 PM | |
Joined: 3/27/2008 Last visit: 4/25/2024 Posts: 1098 Rating: (137) |
I would recommend a simple drive system Sinamics g120C for each motor, with encoders fitted to each gearbox output shaft in order to maintain accuracy. The attached shows a BY340 controller which can read encoders and adjust the inverters by analogue input to ensure they are the same.
AttachmentBy340_e.pdf (254 Downloads) |
Tractor |
|
5/5/2016 12:08 PM | |
Posts: 1529 Rating: (202) |
Instead of doing your application engineering over a public forum, I would think it best to talk to your local Siemens partner about this. |
Follow us on