7/17/2018 5:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Set C2 axis Drive MD P2000 = 5000 & check. |
7/17/2018 9:24 AM | |
Joined: 4/23/2015 Last visit: 11/9/2023 Posts: 76 Rating: (5) |
In case C2 P2000 = 5000 is not enough, try to set P0322 and P0324 to maximum speed as well. |
7/17/2018 2:10 PM | |
Posts: 2 Rating: (0) |
I had increased and decreased C2 drive MD P2000 before but this does not help. The set point of both C1 and C2 becomes different. Thus both run out of sync at that time although C2 speed increases. Parameter P0322 is 5000 and P0324 is not visible. |
Last edited by: SKTP at: 7/17/2018 2:11:06 PM |
|
This contribution was helpful to1 thankful Users |
7/19/2018 5:04 AM | |
Posts: 297 Rating: (41) |
Did you do an NCK Reset after changing parameters? I think the NC scales the speed command to the drive based on P2000 which is read once at startup. HTH, SteveA ...sent from App |
Follow us on