6/1/2007 4:45 PM | |
Posts: 90 Rating: (1) |
Sorry ORIENTE, I need to ask you a question out of this subject ... - Your PCS7 V6.2 is it with Step7 V5.4 or not? Thanx, Ali |
6/1/2007 8:49 PM | |
Joined: 5/19/2006 Last visit: 9/24/2024 Posts: 549 Rating: (107)
|
Well I think there is no PCS7 v6.2. PCS7jumped from v6.1 SP1 to v7.0 WinCC jumped from v6.0 SP4 to v6.2 Dec |
6/2/2007 12:39 PM | |
Posts: 90 Rating: (1) |
I do think the same as well... but, I was surprised from the version mentioned on the....subject line... Thanx, Ali |
6/5/2007 9:49 AM | |
Joined: 11/29/2006 Last visit: 8/18/2024 Posts: 29 Rating: (0) |
here are all the stuff installed on ES |
6/6/2007 10:05 AM | |
Joined: 11/29/2006 Last visit: 8/18/2024 Posts: 29 Rating: (0) |
server diagnose contents |
Follow us on