12/19/2012 6:08 PM | |
Joined: 7/7/2010 Last visit: 4/24/2024 Posts: 14624 Rating: (2348)
|
I usually punt back to Siemens via Support Requestwhen I cannot find the "how" within 5 minutes of searching their web site/forums/FAQs/Manuals/Getting Started Guides/etc. They said the hardware you have is sufficient to the task, so get them to explain "how". I recently modified a GSD/GSE file for a 3rd party torque feedback sensor so I could retransmit to a Siemens drive as actual torque feedback. If I knew the answer to your question, I could have the drive read directly from the torque sensor via profibus, but instead, I have the plc in the middle performing the retransmit. I will have to warn you about the s7-1200 & Siemens SIMATIC drive communications -- the experts are kind of like in knowledge silos. The plc people do not generally know much about how to do drive stuff, and the drive folks tend to only know legacy step 7 stuff. Over the last year, Siemens has been improving that situation, but do not be surprised if you get bounced around a bit and ultimately someone in Siemens HQ has to find the solution you need. |
science guy |
|
12/19/2012 6:22 PM | |
Posts: 34 Rating: (3) |
Thanks huggy, i'll take the route, if I find a solution I will post for others who may be going through the same. |
12/19/2012 8:59 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (150) |
ok, this is a one axis planner and p-reg, it uses position from encoder as input, look if some part is useful for you. p.s. : it was made in Step7 SCL, not TIA. Attachmenttrajplanner.pdf (274 Downloads) |
Follow us on