6/16/2017 9:51 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi Caio. Yes, you can change the attribute and only a compile+download change is needed. Not a full download. Compiling the OS is not necessary. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
3/25/2019 3:50 PM | |
Joined: 12/12/2013 Last visit: 4/30/2024 Posts: 31 Rating: (1) |
Oreca, Is there a specific method for changing the system attributes? Is it done in the library? |
3/25/2019 8:38 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, You can change system attributes in the "Blocks" folder (Open the block, go to input/output section on top and select your input, right click and adjust attributes. For user created blocks in SCL, you can adjust them in SCL editor. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on