1/18/2013 12:36 PM | |
Posts: 3037 Rating: (192)
|
Hello, Here you canfind more information about connection status. How can you visualize the current status of the CPU on a WinCC flexible operator panel? /tf/WW/en/Posts/32198 /tf/WW/en/Posts/75849 Tweety |
1/18/2013 1:27 PM | |
Posts: 3 Rating: (1) |
Thanks Tweety for your response, Just read post from trapper66 /tf/WW/en/Posts/75849 As he wrote - official Siemens response is that there is no a good way to get the system event parameters. So just to let you know, I found a walkthrough for 1 minute scheduler which makes it quite slow to detect connection loose. I made a script which is detecting a connection failure. (as it is written in other posts) I connected it to 1 minute schedule. Additionally I connected it to 14001 System Event so it is "fired" sooner than the 1 minute schedule. Hope that rest of you can use this information. If something is not clear I can explain it. Tomas |
11/24/2015 9:02 AM | |
Posts: 2 Rating: (0) |
Hello, Tomas. I encountered a similar problem. |
12/1/2015 12:52 PM | |
Posts: 3 Rating: (1) |
Hi, I don't really get your question. Please make it clear... |