5/9/2011 3:21 PM | |
Joined: 6/29/2010 Last visit: 10/27/2022 Posts: 112 Rating: (63) |
Hello, The new "System Manual"is avaiable to download: http://support.automation.siemens.com/BR/view/en/36932465 This manual include description about the new features of v2 CPUs like DataLog, Web Server, PROFIBUS, etc.. |
5/10/2011 1:53 AM | |
Joined: 10/7/2005 Last visit: 4/23/2024 Posts: 3004 Rating: (1046) |
unfortunately not all that strange dear Pegaiabut rather the norm. The entry ID stays the same, but now contains the latest version of the manual and older versionsare no longer available which can be annoyingif you want to look up for example module data or system spec's from some years ago (it would be nice if Siemens would also make available previous manual versions at the same link, just like previous firmware versions are all available in one entry). btw, it seems there is a number of youwho are very exicted and simply can't get enough news aboutanything related to the new TIA Portal or S7-1200's etc. etc.. If you are one those,there is alsothe following correction notice to this latest manual availableat the link below: SIMATIC S7-1200 Programmable controller system manual Update to edition 04/2011 |
Cheers |
|
This contribution was helpful to1 thankful Users |
Follow us on