5/4/2020 5:13 PM | |
Joined: 2/1/2019 Last visit: 1/4/2024 Posts: 31 Rating: (1) |
Hi! Any help, please. TIA PORTAL 15. When I trying to create OPC DA tag TIA PORTAL (Runtime Professional) has crashing. Crash report (Link) - [snip] There was creating OPC connection in project - OK There was connecting to OPC server - OK If I trying create HMI tag there is crash, when I choose ADDRES field value (screenshoot) t1 and t2 - it is no tag, but container (like folder), wich TIA cant't open - because crash. OPC SCOUT is monitored the OPC tags on the server. AttachmentFiles.zip (194 Downloads) |
Last edited by: 4phh at: 05/04/2020 17:14:20Last edited by: 4phh at: 05/05/2020 07:37:11Last edited by: Jen_Moderator at: 05/05/2020 08:49:07Removed link and added files as an attachment. |
|
5/7/2020 4:29 PM | |
Joined: 2/5/2013 Last visit: 4/25/2024 Posts: 320 Rating: (74) |
Only need to intsall TIA 15.1 last Update 4 (12/2019) and If you are also using PLCSIM V15.1 then better to install Update for PLC SIM Update 1 (02/2019) Br, AmolG. |
Last edited by: Jen_Moderator at: 05/08/2020 06:50:17Optimized links. Please rate it. |
|
5/8/2020 3:09 PM | |
Joined: 2/1/2019 Last visit: 1/4/2024 Posts: 31 Rating: (1) |
TIA Portal Update Pack 4 was succesfully installed. But the situation not changed. TIA Portal has crashed. Report attached.
Attachment417b9ef3-3d81-4fb4-bfbf-0dc7d016c500.zip (166 Downloads) |
5/26/2020 7:22 AM | |
Joined: 2/1/2019 Last visit: 1/4/2024 Posts: 31 Rating: (1) |
There was created new clean project. New opc connection to OPC DA server. The error was repeated. Added report.
Attachmentb2eba854-b089-45c5-a542-5df8fedc25d4.zip (166 Downloads) |
Follow us on