3/2/2009 12:11 PM | |
Posts: 1776 Rating: (95)
|
Hi, delete the dcf file. see FAQ http://support.automation.siemens.com/WW/view/en/26134056 |
This contribution was helpful to1 thankful Users |
3/2/2009 1:58 PM | |
Posts: 157 Rating: (10) |
Dear April, I do what you say, But nothing changed.. please see the picture bellow.. |
8/25/2009 11:18 PM | |
Posts: 2661 Rating: (279)
|
One way is to open another project by double-clicking the project.mcp file of another WinCC project (found in the project root). BTW, is the following thread related to the same problem? Alarm Logging RunTime hangs up (WinCC 7.0) If yes, I think you should delete it. Regards |
5/31/2011 7:20 AM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
Thanks for the extra info, Komi, I had this once, stopped WinCC by Reset_Wincc.vbs and deleted the archive (cause it was not critical at the time) and got back running afterwards. |
B r g d s , |
|
5/31/2011 9:02 AM | |
Posts: 3 Rating: (0) |
Reset_Wincc, deleting archives and deleting .dcf file didn't help me! If I activate taglogging, it generates the same errer. |
5/31/2011 9:24 AM | |
Joined: 10/3/2010 Last visit: 9/20/2024 Posts: 1562 Rating: (191) |
possibly there might be something wrong with your SQL Server. some things you might wanna give a try if you didn't already: 1. after deleting archives & backup of your actual project, use the project duplicator to save the project under a different name & try that one or 2. found something in this forum to solve another TagLogging issue but maybe it can help you too: Before doing so, make a backup copy of your project and then reset the WinCC archives. |
B r g d s , |
|
Follow us on