1/9/2020 2:58 AM | |
Joined: 3/8/2019 Last visit: 7/11/2024 Posts: 14 Rating: (0) |
Hi Experts, I also experience this kind of problem in my case I migrated WinCC V6 project to WinCC V7.4. And I have a printer that printing every 5 minutes. My problem is the tags that responsible for assigning for printing interval is not created. I check the existing scada that they are still using for the operation, In properties of the IO field for printing interval, the tags was also uncreated like the tags that I migrate to WinCC V7.4 but they can able to assign the time for printing interval. I have try to upload the program from the plc to check the tags so that I can manually add the tags to scada but the problem is the program is in STL code which is I am not good at this programming language because I only use Lad in programming. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/09/2020 20:33:20New subject after splitting |
|
Follow us on