8/22/2013 8:14 AM | |
Posts: 30 Rating: (0) |
Hi LOGO! users, Can you tell me if is possible create binary code with LOGO!TD funkcion key. For example: F1 key set program for external unit: - first click set binary 000 =>program0 - second click set binary 001=>program1 - third click set binary 010=>program2 etc. but i have now only 3 programs. Thank you so much for every help. Attachmentimg-822074339.pdf (209 Downloads) |
Last edited by: PeTer111122 at: 8/22/2013 8:48 AM |
|
8/22/2013 11:45 AM | |
Posts: 30 Rating: (0) |
Hi Ste39, Yes, i did it so as you write, but i am not sure if is possible in the future expand on more output. For example: Now i have only 2 outputs because i have 3 programs (00,01,10) now its working correct. But, if i will have 3 autput = 3bits & 2^3=8 programs. (000, 001, 010, 011,.. etc.) first counter must be 2 times ON when was first click and fourth click.
AttachmentSoftware_koncova montaz_EY-1356.zip (207 Downloads) |
8/22/2013 12:14 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, You could use the BCD code program( or part of), that our friend Betel wrote. See attachment. Regards, Marcjan AttachmentBCD Pulse an Ausgang.zip (222 Downloads) |
Last edited by: Marcjan at: 8/22/2013 12:15 PMProblem solved? |
|
This contribution was helpful to1 thankful Users |
8/22/2013 12:51 PM | |
Posts: 30 Rating: (0) |
Thank you so match MarcjanThis way is amazing |
8/23/2013 1:23 PM | |
Posts: 30 Rating: (0) |
HiMarcjan, I have next question: if i want send to vision sensor PROG04, i must set output Q1&Q2..Qn. For example: PROG06 is BCD code 101 and next step i must send to vision sensor PROG02 this is BCD code 001. My question is: Is it posible convert decimal number to BCD code ??
|
8/23/2013 1:36 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Yes it's bin done before See: Binary value on outputsRegards, Marcjan |
Problem solved? |
|
Follow us on