2/13/2010 8:26 PM | |
Posts: 99 Rating: (3) |
Dear experts, If I select "Alarms" as default display mode in the Text Display Wizard, then when an alarm is activated, the TD200 does not show it until it return to the alarm screen up to 1 minute later. I have made a test application. Download in the PLC, run it. Prepare to put 1 at V50.0 or V50.1 in the chart screen in MicroWin then go in a user screen in the TD200 (test or test2). Put V50.0 or V50.1 at 1 and nothing append for up to 1 minute. What should I do to make the TD200 react faster to an alarm? TD200: V3.0.2.2 6ES7272-0AA30-0YA1 MicroWin: V4.0.6.35 CPU:224XP Rel.02.01 Attachmenttest2.zip (190 Downloads) |
11/24/2017 2:18 PM | |
Posts: 1 Rating: (0) |
How I can change this time? Our TD200 have this time 10 sek, but I would change it back 1 minute. |
Follow us on