4/6/2018 9:37 AM | |
Joined: 5/12/2006 Last visit: 4/19/2024 Posts: 22211 Rating: (2979)
|
Hello, is the ALM in state for Operation? Christoph |
4/6/2018 10:01 AM | |
Posts: 12 Rating: (0) |
In the ALM r2 is set to 42. |
4/6/2018 11:40 AM | |
Posts: 12 Rating: (0) |
The input word is set like so: 2#0000_0010_1100_0000 Which I guess with some byte swapping the module is reporting ready for operation on ZSW1.1. |
4/6/2018 11:54 AM | |
Posts: 12 Rating: (0) |
OK, I've now got it working. So I needed to use the mapped I/O rather than block read and write instructions. Many thanks for all your help. |
Follow us on