2/17/2020 5:25 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
Question: The LOGO! cannot directly process a type K thermocouple. Do you have an external converter with a 0-10V output? If not, then it doesn't work. If so, then I have a program proposal (see attachment). On the LOGO! display you can change the time value and the difference of the required temperature increase. AttachmentIgnition_monitoring_FS4.zip (184 Downloads) |
This contribution was helpful to1 thankful Users |
2/17/2020 8:15 AM | |
Joined: 12/18/2014 Last visit: 4/25/2024 Posts: 32886 Rating: (4066)
|
I wish you also a good day ... |
Follow us on