11/12/2016 10:56 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
No, to my knowledge it is not possible. The only way I see is to create your own message text with priority 0. After each reset, the message text is reactivated and the time and date of the reset are displayed. If several message texts are activated at the same time, the message text with the highest priority is displayed. AttachmentVarmestyring_V6.3_Final.zip (287 Downloads) |
This contribution was helpful to1 thankful Users |
11/12/2016 11:11 AM | |
Posts: 67 Rating: (7) |
Thanks, I'll give it a try on the device, to see how it behaves. |
This contribution was helpful to1 thankful Users |
11/12/2016 11:44 AM | |
Joined: 12/18/2014 Last visit: 4/26/2024 Posts: 32887 Rating: (4066)
|
When you do this, my suggestion does not work anymore with the own message text for the reset Display. |
11/13/2016 8:44 AM | |
Posts: 67 Rating: (7) |
Got a little further in this. Now there should appear a warning to order fuel when 400 hours is reached (set to 1 minute for simulation) It's actually quite fun to play with this little device. I am overwhelmed by all those possibilities. Everyday i got a new idea, with a feature to add.. Maybe i should remove "final" from the filename I guess there will never be a final version. LOL I'll still have to work with a timestamp, so i can see, when i last ordered fuel. AttachmentVarmestyring_V6.2.1_Final.lsc.zip (298 Downloads) |
Last edited by: cs_dk at: 11/13/2016 8:45:54 AM |
|
11/14/2016 5:51 PM | |
Posts: 67 Rating: (7) |
Think I got it now.. 0 is not highest priority, in my world it would be.. The LOGO! seems to have a different opinion.. I think it works now. Until I find another feature, that would be nice to have. It will switch from red to amber diaplay, when night setting is on, but i can live with that. The message will appear, and that is most important.. AttachmentVarmestyring_V6.2.2_Final.lsc.zip (336 Downloads) |
11/16/2016 7:38 PM | |
Posts: 67 Rating: (7) |
Add'et a timer for daily start.. The temp is displayed as auto, but it is the day temp setting. I just wanna make sure no one alters the settings. There for the "Auto" (keep your fingers away) message. It should run for some time, and if i don't switch on the day switch - Well, then there is no car on my lift, no work should be done, and it can go to night mode again. If there is something in the garage, then it will have preheated some time before i enter. Win win. :) Will have to see, if it works tomorrow. AttachmentVarmestyring_V6.2.3_Final.lsc.zip (313 Downloads) |
12/11/2017 9:37 AM | |
Joined: 6/19/2017 Last visit: 4/26/2024 Posts: 7954 Rating: (162) |
New question published by telegramteknik is split to a separate thread with the subject Want to use a PT1000 sensor, which parameters do have to change?. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on