9/21/2014 3:18 PM | |
Posts: 247 Rating: (2) |
Hi Ralfinio, I want to generate synthesis temperature profile as per attached file. I never used Cascaded Polygon block. Please check the graph i have to create in the attached file.
AttachmentTemp_SP_generator.pdf (316 Downloads) |
Last edited by: Min_Moderator at: 9/22/2014 1:53 PMHere is the right link /tf/WW/en/Posts/107161 Last edited by: Min_Moderator at: 9/22/2014 1:50 PMNew subject after splitting from |
|
9/22/2014 3:18 PM | |
Posts: 247 Rating: (2) |
Hi Ralfinio, Currently i dont have the CD as i am on site If you have it can you attache it here in any small demo project these fbs i really need. Thank you
|
9/22/2014 9:04 PM | |
Posts: 247 Rating: (2) |
Hi Noname, I have PCS7 V8.0 sp1 licence and software only the thing is that may be some conflict in FBs. |
9/23/2014 8:59 AM | |
Posts: 567 Rating: (106) |
Hi RaviS, attached you can find the POLYG_P block from PCS 7 Standard Library V7.1 SP3. AttachmentPolygon.zip (282 Downloads) |
This contribution was helpful to1 thankful Users |
9/23/2014 12:09 PM | |
Posts: 247 Rating: (2) |
Hi Ralfino, Thanks for FBs, i will check and will revert back to you. Thank you so much. |
Follow us on