12/5/2020 12:30 PM | |
Posts: 9 Rating: (0) |
I honestly believed that it was always the same LStack vector that was used and overwritten and reallocated, but I was "partially" wrong. In fact, as can be seen from the attached FAQ, the Temp area of each block is "appended" and nested ... Good! Local data addressing with S7-300 / S7 400 - ID: 291495 - Industry Support Siemens |
12/7/2020 4:21 PM | |
Joined: 7/7/2010 Last visit: 9/18/2024 Posts: 15202 Rating: (2417)
|
I would not generalize TIA Portal's compiler results based on anything specific to S7-300/400 PLCs. In fact, I would question if they were the same. That said, what PLC architecture are you targeting the next project?
|
science guy |
|
12/7/2020 5:35 PM | |
Posts: 9 Rating: (0) |
S7-1500 CPU. As I told I had some tests (very stressfull for temporary variales) and It seems to work in the same way. It seems....
|
Follow us on