9/12/2021 9:05 PM | |
Joined: 12/18/2014 Last visit: 9/19/2024 Posts: 33793 Rating: (4197)
|
What art of control do you want? 3 point step controller? Or PI controller? |
9/12/2021 9:08 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
I want to control the temperature of a Jacuzzi from 0 to 40 degrees on the HMI panel |
9/12/2021 9:10 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
my heater is controlled by a digital output |
9/12/2021 9:13 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
I want digital output |
9/12/2021 9:19 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
Yes. set a desired temperature and the heater is on until the water is hot. |
9/12/2021 9:21 PM | |
Joined: 5/25/2020 Last visit: 3/16/2024 Posts: 32 Rating: (0) |
my HMI is KP 400 I want two buttons one for temp up and one for temp down |
Follow us on