1/17/2018 11:52 AM | |
Joined: 2/16/2016 Last visit: 3/28/2022 Posts: 7 Rating: (0) |
Hello All, I finally make it works after formatting the memory card. |
This contribution was helpful to1 thankful Users |
3/10/2019 7:22 PM | |
Posts: 5 Rating: (0) |
Hi, PLC : S7-1200 -> CPU 1214C DC/DC/DC FAULT: ID event 16# 2A05 :FFEF Solution : Online -> Functions -> Reset to factory setting |
4/5/2023 8:59 AM | |
Joined: 1/12/2023 Last visit: 5/13/2024 Posts: 19 Rating: (0) |
Hello, Yes, I had the same problem when I try to change the name of software PLC (see in attachment) and I forgot some Input Forced, they give me the Error "Test & Commissioning Function Active" , after that I was going online to deactivate the Forced Inputs and I was able to download with the new name. AttachmentTest & Commissioning Function Active.pdf (531 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on