4/5/2023 8:59 AM | |
Joined: 1/12/2023 Last visit: 3/12/2024 Posts: 19 Rating: (0) |
Hello, Yes, I had the same problem when I try to change the name of software PLC (see in attachment) and I forgot some Input Forced, they give me the Error "Test & Commissioning Function Active" , after that I was going online to deactivate the Forced Inputs and I was able to download with the new name. AttachmentTest & Commissioning Function Active.pdf (371 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on