6/12/2009 10:37 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
How can I test os client on Engineering station? |
6/14/2009 11:33 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
Is it possible to test os client in ES computer?and how? |
6/14/2009 9:11 PM | |
Joined: 4/5/2006 Last visit: 3/13/2024 Posts: 917 Rating: (63) |
Hi SM, i'm alil confised about your new question if you want want ran "OC Client" on your ES Station you only nned create a "PC Station" on your ES with "WinCC Application Client" (as well as standard client) Easterngave you a full manual to do this (expecially 2nd link) if you are asking for something different, explain please Regards |
6/30/2009 9:10 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
Instead of OS simulation,It may be simulate "os server" with creating an additional os client (in addition of existing os) and run it onES computer.Isit possible? You can check the response of Phantom75in /tf/WW/en/Posts/22617 |
Follow us on