4/16/2013 7:09 PM | |
Joined: 8/25/2006 Last visit: 1/26/2021 Posts: 2005 Rating:
|
Hello. While complile, you have problems with the library versions used in project. You need to update your libraries to the latest available versions. Go to the CFC-menu 'Options-Block Types', you will see the window with libraries installed on hard drive (left part of the window) and libriries imported to the project (right side of the window). By selecting the library in the left side and press 'New Version' you can update each library imported into the project to actual version, after that you should compile without errors, download new program and will not have the problems with change memory. Also look at these threads on how to operate with libraries: and search inside conferenceSIMATIC TDC, FM458, T400.
|
This contribution was helpful to
2 thankful Users |
Follow us on