5/16/2012 6:02 AM | |
Posts: 4 Rating: (0) |
Hello! I don't know weather the step7 V5.5 and WINCC V6.2 sp3 compatible or not And hope somebody can help me. |
5/16/2012 6:17 AM | |
Posts: 1064 Rating: (72) |
they are 2 different programs and can be installed on the same machine but it has to windows xp sp2 or 3 |
This contribution was helpful to1 thankful Users |
5/16/2012 6:25 AM | |
Joined: 3/18/2008 Last visit: 12/8/2023 Posts: 1750 Rating: (272) |
As said by Playerslight, Please ensure OS-Windows XP SP2/SP3 Also Check Following for the Comapatibilty list for siemens software. Are there lists for the compatibility of Microsoft operating systems and SIMATIC Software products? Hope this helps.i |
VANDE MATARAM..... |
|
5/16/2012 8:41 AM | |
Posts: 1064 Rating: (72) |
both softwares will run xp sp3 .I have 3 systems running on xp sp3 right now |
5/17/2012 2:47 AM | |
Posts: 4 Rating: (0) |
It's a new Project. It has to be ordered by owner. In this case I think I can use it to finish the project. Thank you all! Best regards |
Follow us on