2/20/2020 7:19 AM | |
Joined: 4/23/2016 Last visit: 3/22/2024 Posts: 1 Rating: (0) |
Sir, i am using TIA PORTAL V15.1 I am facing the problem with UMAC meta. I make a project and protect the project with this security of my project with administrator rights. after again opening the project the project asked the user id and password that is ok. but when I copy the project in different computer the project showing logon error. the installed UMAC accesses control configuration meta one or more product packages is not compatible with the UMAC meta used for creation of the project. thanks Irfan Khan Pathan
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/20/2020 14:21:03New subject after splitting |
|
9/14/2021 5:05 AM | |
Posts: 1 Rating: (0) |
dear sir, I can be facing the same issues plz support clear solution |
10/6/2021 12:55 AM | |
Joined: 8/8/2020 Last visit: 3/4/2024 Posts: 2 Rating: (0) |
|
Last edited by: googl at: 10/06/2021 00:57:02 |
|
10/6/2021 1:00 AM | |
Joined: 8/8/2020 Last visit: 3/4/2024 Posts: 2 Rating: (0) |
|
Follow us on