8/4/2020 8:05 PM | |
Posts: 7 Rating: (0) |
Good day! Please help with the solution of the same problem 8180 of the MB_MASTER block! I tried all the recommendations that I found on this forum, as well as on the Internet, but nothing helps. Controller S7-1200, TIAPortal V15.1. I'm new to this. I check in simulation, compile, load into the controller, press RUN / STOP - it does not help. The "Optimization ..." checkbox is unchecked for blocks (screenshots). I am attaching screenshots. PS. Modbus RTU did it based on this video - https://www.youtube.com/watch?v=eH3UUMKy_I0 - but in the video everything works, but I don't ... ------------------------------------------------------------------------------------------ AttachmentError 8180 MB_MASTER.docx (633 Downloads) |
Last edited by: Andry_SS at: 08/04/2020 20:11:14Last edited by: Jen_Moderator at: 08/05/2020 10:01:54New subject after splitting Last edited by: Andry_SS at: 08/08/2020 06:23:31 |
|
8/8/2020 6:15 AM | |
Posts: 7 Rating: (0) |
Please help me! Where are all the specialists? |
8/10/2020 4:50 PM | |
Posts: 7 Rating: (0) |
The problem is still not resolved ... |
8/10/2020 9:29 PM | |
Joined: 3/30/2020 Last visit: 4/19/2024 Posts: 4414 Rating: (924) |
Hello. The error message (8180) says: "Invalid value for the port ID". You say: "I check in simulation". Are you simulating with PLCSIM? You need actual hardware. PLCSIM does not work for Modbus RTU. The S7-1200 is the master - what is the slave? How does your connection look like? Regards. LATE ADDITION.. What happens if you use actual hardware? |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to1 thankful Users |
8/23/2020 8:37 AM | |
Posts: 7 Rating: (0) |
Dear qwazee! I do not have operating equipment yet, but it will be purchased a little later. I really do the simulation programmatically on PLCSIM. I assumed that the Modbus port most likely did not work on PLCSIM, but, unfortunately, I didn’t know for sure, and no one suggested it. This is my first time programming Siemens controllers. Thank you for taking the time and confirming with screenshots! Hope you are 100% right, and when the real hardware arrives, this port error will be gone! Thank!
|
This contribution was helpful to2 thankful Users |
5/10/2022 12:35 PM | |
Joined: 5/10/2022 Last visit: 3/11/2024 Posts: 1 Rating: (0) |
use mobus below do not use mobus rtu above i fixed it |
2/13/2024 6:35 AM | |
Joined: 2/13/2024 Last visit: 2/15/2024 Posts: 1 Rating: (0) |
Thank you for advice ! It is worked for me ! |
Follow us on