Industry Online Support
Technical Forum
11/21/2012 7:45 PM | |
Posts: 11 Rating: (0) |
Hello, I am new to the entire system and I have a work involving the use of HSC. Now, I have gone through this enttire thread and i still dont understand. i have 2 inputs A and B from my quadrature encoder. I need to not only count but specify if A is leading or |B is leading to clarify the direction of motion. I dont even understand where all the MW,MD and ID are coming from. With thr HSC DC, where can i get the output count for and also to retrieve the former value of 1 of the input points, how do i do that? Please, I really need this. Thanks for the help in advance. Please, I am using V11 update 2.0. Can someone send me a sample project. I tried all i hints and tips given on this thread but the HSC counter is not energizing even with input pulsres...
|
Last edited by: O_Moderator at: 11/22/2012 9:39 AMnew subject after splitting from /tf/WW/en/Posts/67379#top |
|
11/22/2012 9:42 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Thread closed, because question is already published in the following thread use of HSC. Best regards O_Moderator |
Follow us on