2/2/2012 2:27 PM | |
Posts: 56 Rating: (1) |
Hello Is there any example program to connect Siemens PLC 314C-2DP to Lenze Servo drive 9300 via Profibus protocol ...??? |
2/2/2012 2:42 PM | |
Joined: 4/22/2010 Last visit: 2/15/2024 Posts: 5697 Rating: (711)
|
Hello, Better have a look at the Lenze site for that. http://akb.lenze.de/AKB-englisch/infopool.nsf/html/index-inhalt Look at downloads for S7 examples. Regards, Marcjan |
Problem solved? |
|
2/2/2012 2:53 PM | |
Joined: 3/21/2006 Last visit: 4/4/2024 Posts: 10228 Rating: (1181) |
You will reach finally the same as suggested Marcjan but try it - put 'lenze' in search field here in forum... Best regards, Hristo Mihalev |
2/2/2012 3:02 PM | |
Posts: 56 Rating: (1) |
Is there somebody has knowledge or experience in this topic ...??? |
2/3/2012 7:28 AM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (221) |
Check this - Connecting a SINAMICS drive to an S7-1200 CPU in TIA Portal (via GSD file) The only difference here with respect to your requirement is that you are gonna insert the GSD file of Lenze drive in place of SINAMICS drive. Rest remains the same in S7-1200 side and ensure the settings / parameterization is done correctly in the Lenze drive end. Keep us posted here on the updates of your trials / success |
Last edited by: Ganes10 at: 2/4/2012 6:21 AMLike it? Rate it! |
|
Follow us on