2/1/2012 4:47 PM | |
Joined: 7/7/2010 Last visit: 4/24/2024 Posts: 14624 Rating: (2348) |
Perhaps this link will help you spend your money wisely : http://www.omega.com/temperature/Z/ThermocoupleResponseTime.html Having a sample of 400 Hz when the response time may be no better than 1 sec is a rather expensive approach. RTD is for more accurate or up to moderately high temperature input (<800C). TC is cheaper and faster andless accurateand can read > 800C. Maybe this will help. http://www.jimpinto.com/writings/tempsensors.html I have had this discussion many times. We usually go with TC input and update @ 10-20Hz. We often want 1000Hz, but that's not realistic and can be misleading. |
science guy |
|
Follow us on