8/25/2016 10:11 AM | |
Joined: 10/26/2011 Last visit: 4/22/2024 Posts: 760 Rating: (190)
|
Hello, you have two possibilities: 1. New installation of the PC 2. Contact the Technical Support. To 1. To 2. If you contact the Technical Support, please use following link: |
SIMATIC PCS 7 - Overview |
|
11/17/2016 7:30 AM | |
Joined: 3/14/2008 Last visit: 4/24/2024 Posts: 2065 Rating: (926)
|
Hi Ventouris, What are you meaning exactly when you say: Client station? I hope you are talking about one of the following: - OS Single Station - OS client - Web Server - Web Client - Information Server - Batch client - Route control client - OpenPCS7 Standalone - OpenPCS7 with client - OpenPCS7 OS Single station These are the only station where you can install Windows 10. What Windows version do you use? Because the only released version is: Windows 10 LTSB 64bit. With this, there are a few footnotes on the Windows 10: - Intel Teaming is not possible - When using two network cards, one with a default gateway and one without, problems can occur and terminate the connections. Siemens recommends using one network card only. According to your text, you installed Step7, but this is not needed when using on of the released stations above....
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on